CAP#.EDGE

Description

Selects which edge of the trigger input to use.

The trigger source is monitored for either a rising, falling, or either edge. When one of these edges is detected the position or time is captured. This setting is always used irrespective of the precondition configuration.

Examples

Usage

1: Rising edge (default)

2: Falling edge

3: Rising or falling edge

Code

-->CAP1.EDGE 1
-->

Context

For more information please refer to Capture.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

1 to 3

Default Value

1
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
CAP1.EDGE

4400h

01h

Unsigned8

-

-

Read/Write

No

CAP2.EDGE

4401h

01h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

CAP1.EDGE

31020

792C

Unsigned8

Read/Write

-

CAP2.EDGE

31021

792D

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

CAP1.EDGE

31020

Unsigned8

Read/Write

-

CAP2.EDGE

31021

Unsigned8

Read/Write

-

Related Topics

Capture

CAP#.PREEDGE